This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] OPT3001: What is the f1' value of the OPT3001?

Genius 9155 points

Replies: 1

Views: 797

Part Number: OPT3001

  • The concept and definition of F1' is explained well in the following paper: 2004_Goodness_of_Fit_Photometers.pdf(web source).

    In response to this request, data was taken on 5 units, at room temperature, at one time, with a spectrum from 300-1000nm in 5nm steps, and the F1' values were as follows for those particular 5 units:

    13.7%
    11.1%
    12.6%
    10.4%
    10.6%

    This is not a guarantee of past, current, or future performance. TI makes no warranties and assumes no liability for applications assistance or customer product design. You are fully responsible for all design decisions and engineering with regard to your products, including decisions relating to application of TI products. By providing technical information, TI does not intend to offer or provide engineering services or advice concerning your designs.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.